Share via email
Some fields are missing
send eMail

Hysteresis

The maximum difference of the fluid output signal as it passes through the full electrical input signal range in the upward and downward directions; stated as a percentage of the maximum fluid output signal (the flow rate is assumed for the example in the sketch).

Hysteresis is caused by friction and magnetization.

My Comparison List