Here you will find a short list of our most frequently asked questions. If you have a question that is not answered, please do not hesitate to contact us by telephone or e-mail.
Product information
Using the search function (type or article search) by typing in a Bürkert type or article or by using the navigation in "Products & Application".
Type in your Bürkert product type (eg. 6213) within the search function. There you will find a filter for "Downloads" or you can go to the “Type Detail Page” where you will find a download section with all related documents for your product.
Type in your Bürkert product type (eg. 6213) within the search function. There you will find a filter for "Downloads" or you can go to the “Type Detail Page” where you will find a download section with all related documents for your product.
Type in your Communicator-supported Bürkert-type (i. e. 8741) within the search-function and enter the type-detail-page. There you have a download section where you will find the Communicator-software for your product.
EDIP (Efficient Device Integration Platform) is a device platform for intelligent connections. Read more about EDIP.
The term “Industrie 4.0” stands for a new industrial age in which industrial processes can be carried out in a consistently digitized manner. We support this development with its device platform EDIP (Efficient Device Integration Platform) that enables intelligent networking down to the sensor and actuator level.
Approvals of certified products can be found on the website of the relevant institution:
The previous product information search in the MyBurkert area is now integrated in the regular search function on top of the page.
Yes! You can configure a valve island of Type 8652 AirLINE yourself. Call up the type – e.g. via the search function – and start your first configuration.
At the bottom of the configuration tool, you can see your individual configuration code at any time.
Click on the “three dots” next to the configuration code to open a pop-up box from which you can copy the number.
Under this, you can see the result of your most recent work.
Entering the code in the search bar of our website will take you to your most recent work status.
Here, you also have the option of forwarding the link to your configuration.
This allows you to share your result with your colleagues or a Bürkert employee.
When you enter the code in the search, your most recent work is called up.
The validity date of your configuration also appears.
This is only necessary if you log in after configuring your desired product to complete your order.
After confirmation, you will be shown your customised price and the shipping date for your configuration.
Functions
If you accept our cookies, we can provide you with the optimal service on our website. Click on the following link to receive further information about which kind of cookies are used and for what reason they are stored in our "Data-Privacy-Policy"
Yes, you can order products easily using our eShop once you are registered. To do so please register yourself. Take a look at our short e-Shop video to learn about the advantages of registration and online ordering:
You can register for the eShop using the LogIn button at the top right hand corner of the website. If you are an already an existing Bürkert customer, you can register quickly and simply by entering your customer number and any invoice number:
If you are still unable to order after you have fully activated your customer account (including setting your password), please contact us. We will try to solve the problem as soon as possible and apologize for the inconvenience!
You´ll find prices, delivery notes, invoices, contacts etc. in main the navigation point „My Burkert“.
You can enter your article number or type number directly into the search box or type in a particular search term. After entering the third character, an autocompletion result will appear, providing your search keyword or phrase is available. You can then select the required item or description from the options provided.
Yes, our Quick Order is the simple and fastest way to fill your shopping cart. You have three options to put Bürkert products in the shopping cart using Quick Order.
You can find the video on our Bürkert Quick Order function here:
1. Via the “identification number”: Enter the identification numbers in the designated fields, then adjust the quantity and use the button to add everything to the shopping cart. You can download the list for checking or save the items in an individual watchlist.
2. Via the “CSV/Excel documents upload”: Drag your file into the designated field or use the button to search your computer. Your file should display the following formatting:
Format: Excel or CSV
two columns
Column 1: identification number (required)
Column 2: quantity (optional)
If your file displays more than two columns filled with data, only the first two columns will be edited anyway.
If your file only displays one column, but it is filled with identification numbers, it can be edited, the item quantity is then stated to be 1.
3. Via “Copy & insert”: Enter the identification number and quantity per line in the input window and press the Enter key after every line. An example of the input format is highlighted in grey in the input window. Next, confirm your selection with “Accept input”.