Share via email
Some fields are missing
send eMail

Full scale value range/nominal flow rate

The full scale (F.S.) value range is the range of possible measuring range limits.

The minimum value is the smallest possible full scale value for the nominal flow rate while the maximum value is the highest possible full scale value for the nominal flow rate. Any full scale values between these are also possible of course. The specifications refer to defined reference conditions (for example, standard liters per minute or standard cubic centimeters per minute).

My Comparison List