Share via email
Some fields are missing
send eMail

Explosion-proof coils

The mechanical construction and coil design of explosion-proof coils are similar to those of DC coils.

Corresponding measures, for example, pressurized enclosure or potting of electrical components, are used to ensure that explosive sparks cannot escape to the outside and thus trigger an explosion, even in the event of damage. The coil systems are generally operated with direct current by means of a generally press-fitted bridge-connected rectifier in the coil.

Bürkert offers a wide variety of different coil systems which can be combined with many different fluid modules on the basis of a modular principle. See the "Approvals" section for further information on explosion protection.

My Comparison List