Solenoid valves with energy-saving kick and drop coil
Durable, silent and energy-saving: how the Kick and Drop coil not only allows you to save money, it allows you to protect the environment as well.

Media such as fluids or gases must be shut off, released, dosed, distributed or mixed. These tasks are among the tasks undertaken by solenoid valves. This means that they are subject to countless requirements in a wide range of different application environments. The challenge for the future lies in a sustainable and energy-saving solenoid valve solution.
Controlling media with energy-saving solenoid valves
Valves with electromagnetic coil systems are widespread in order to automatically control gaseous and liquid media. Their energy efficiency, lower noise emissions and associated long maintenance intervals are becoming more and more important today. Coil systems with Kick and Drop electronics assemblies rely on improved valve performance, energy saving and new milestones with regards to their efficiency.
The solenoid valves with the new Kick and Drop technology are 35% smaller than conventional valves, but just as efficient. Moreover, Kick and Drop prevents environmental impact from occurring, as they work silently and do not cause any unpleasant mains humming or whistling.

What lies behind the Kick and Drop electronics assembly?
The Kick and Drop coil is a coil with double winding. It consists of an inrush winding and holding winding. In a Kick and Drop electronics assembly, the coil is excited by a high electric impulse. This generates the required inrush power, which the valve needs in order to open. After approx. 500 milliseconds, the Kick and Drop electronics assembly switches to an energy-saving holding power. This then drastically reduces power consumption. The coil is therefore particularly suitable for valves that are open for long periods while in use, such as valves for protecting gas or tap water.

A: The overexcited inrush winding generates a very high starting power over approx. 500 ms
B: The holding winding is connected in series to the inrush winding after 500 ms and reduces the current, and thus the energy demand
Diverse application areas
The areas of use for the Kick and Drop coil are very diverse, and they are used particularly frequently in the installation and heating sector. The Kick and Drop coil can be used anywhere where the following conditions need to be met:
- Energy should be saved
- Water that contains a particular amount of lime must be controlled
- In buildings where faults must be excluded by electromagnetic fields
- Anywhere where fluids and gases to be controlled must not be additionally heated by the coil
- Anywhere where continuously active solenoid valves, such as gas or tap water safety valves, are operated in buildings
- Anywhere where particularly battery-buffered drainage systems are used, to guarantee a longer, safer operating time
Every added value has a benefit for you
More advantages that you can enjoy when using solenoid valves with Kick and Drop technology:
Example calculation
Which solenoid valve with Kick and Drop technology suits your application?
Find the right solenoid valve for your application and get started now to save energy.