Experts in WFI-loop systems: Bürkert
A Water for Injection (WFI) loop is a closed circuit that is used in the pharmaceutical industry for the distribution of highly purified water that meets the stringent regulatory requirements in accordance with the European, American, and Chinese pharmacopoeias (Ph. Eur., USP and ChP) and is obligatory for the production of pharmaceutical drugs. The WFI circuit ensures the availability of purified water of the highest quality.

WFI loop: The heart of a pharmaceutical production facility
A WFI loop is used not only for the distribution of water for injection (WFI), but also for controlling and monitoring numerous quality-dependent processes in the pharmaceutical industry. Purified Water (PW) and Highly Purified Water (HPW), also known as pharma water, or pharmaceutical water, must meet the highest purity standards, and is used in many critical applications. It is therefore essential to have a well-designed and monitored WFI loop to ensure product quality and compliance with regulatory requirements in the pharmaceutical industry.
What are the key considerations when it comes to WFI loops?
There are several key factors that must be considered to ensure the efficient and safe operation of a WFI loop:
Critical factors in WFI loops
Biofilm
One of the main issues in WFI loops is the formation of biofilms. These are formed by microorganisms that accumulate on the inner walls of the pipes and contaminate the water. The formation of biofilms can be prevented through careful monitoring of the flow velocity and water temperature.

Flow profile
The flow profile within a WFI loop must be turbulent to ensure an even distribution of water. A laminar flow profile or the existence of dead zones can lead to the accumulation of dirt particles and microorganisms.

Flow velocity
The flow velocity is another critical factor. This must be set to a velocity that prevents contamination and maintains maximum pump efficiency. However, if the flow is too fast, this can lead to increased wear of the pumps, as well as higher energy consumption or unnecessary pressure drops.

Our solution: FLOWave
The Type 8098 FLOWave flowmeter from Bürkert presents an innovative solution to the challenges faced in the context of WFI loops. FLOWave uses SAW (Surface Acoustic Waves) technology for contactless flow measurement. It has the following advantages:
Holistic, intelligent solutions
The combination of FLOWave and unique Robolux double diaphragm technology creates entirely new possibilities for ultra-hygienic extraction of WFI from the loop:

“FLOWave is not just a flowmeter, but a completely unique instrument for quality assurance.”