Share via email
Some fields are missing
send eMail

Switching test gases safely

Compact valve cluster for leak testing – cooperation with aprotec GmbH

Success Story, die eine Prüf-Anlage von aprotec zeigt

Compact distribution station for automatic tightness testing system

Where fluids are involved, valves for controlling gases or liquids are a must. This is because a wide variety of processes rely on them – from water and wastewater treatment to the food and pharmaceutical industries, through to cosmetics production, petrochemicals, and hydrogen applications. Valves are also essential in many testing applications. For example, in testing systems for air conditioning units, the piping must be checked for tightness to ensure that the coolant does not escape. Such leak testing systems require valves that guarantee a high degree of tightness, are robust and durable and offer substantial throughput in a compact design.

Did you know?

– aprotec GmbH, with headquarters in Karlstadt, Bavaria, specialises in innovative solutions for automation, process systems and leak test technology – the systems are used, for example, in plants for growing ultra-pure crystals for chips used in e-mobility – the Karlstadt-based company also has a wealth of experience in systems for leak testing and, working in close cooperation with its customers, develops solutions tailored to their respective requirements

Mitarbeiter von Aprotec steht vor Prüf-Anlage

Summer, sun, holidays – what more could you want! However, when the sun is blazing down on a motorhome or campervan in midsummer with no shade in sight, an air conditioning unit is essential. There is a wide selection of cooling devices for mobile use, and a common feature among the various models is that prior to being used, they must be tested to ensure long-term reliable operation. This is often performed manually: a special sniffing sensor is held against each connection point to check the piping for tightness.

However, the values obtained through these manual measurements are not reproducible and can be unreliable due to variations in measurement distance and speed. Sometimes, the employee carrying out the check simply passes over the test area too quickly. For this reason, aprotec GmbH has now developed a test system for Truma, a company that manufactures motorhome air conditioners. The system automatically checks the piping of the devices for tightness, thus avoiding potential human error by the person operating the sniffing sensor.

Schnüffel-Klammer von der aprotec GmbH

Sniffing clips replace manual testing

An important element in this are the so-called sniffing clips, which are manually attached to all the connection points of the pipes to be tested. Firstly, an additional sniffing clip that is not involved in the actual testing process measures the background present in the air conditioning unit. If this is within the desired range, the air conditioning unit is initially evacuated to a vacuum of about 1 mbar absolute, and then the test gas (either forming gas or helium) is introduced into the air conditioning unit at a pressure of 40 bar. In the subsequent coarse leak test, all sniffing clips are attached to the detection device, and each clip is then tested individually, with the background measurement checked each time to determine the leak rate at each clip.

 

Valve cluster with 12 flapper valves

If any forming gas or helium escapes at a leak point, the gas is conducted through integrated transfer capillaries in the sniffing clip to the detection system, where it is flagged up. The task of safely switching between the individual clips is handled by a valve cluster. “At this point, there are 12 flapper valves from Bürkert Fluid Control Systems”, explains Michael Landgraf, Managing Director at aprotec. All the sniffing clips are connected to these valves via transfer capillaries. The valves switch in such a way that the transfer capillaries are sequentially connected to the detection system, thereby ensuring that the sniffing clip at a leak point can be clearly identified. The rapid switching behaviour of the Bürkert valves also enables a stable measurement process. The operator who places the sniffing clip on the air conditioning unit receives a visual status notification of the test at the clip. A calibration standard can be attached to the clips, and system calibration is then performed automatically.

The type 0331 valves are robust and have already proven their durability and reliability in many other applications.

 

Michael Landgraf, Geschäftsführer bei aprotec

“We have been working with the fluidics specialists at Bürkert for many years and are impressed with the quality and reliability of their valves.”

Michael Landgraf, Managing Director at aprotec
Ventilblock bestehend aus mehreren Bürkert Ventilen in einer Anlage von aprotec

Compact valve cluster serves as distribution station for the test gas.

Compact with high throughput

The valves used are direct-acting, media-separated pivoted armature valves and are available in 3/2- and 2/2-way variants.

  • 3/2-way version as a distributor or mixing valve
  • Robust pivoted armature, long service life
  • Different diaphragm materials and circuit function
  • Housing available in brass, stainless steel, PEEK or polypropylene
  • Made of highly chemically resistant epoxy-coated solenoids
  • Also suitable for critical media such as aggressive acids and alkalis
  • Type 0331 with manual override for commissioning and testing
  • Switching status via position feedback as binary or NAMUR signal
  • Optionally with electronic power reduction or as pulse variant for energy saving
Bürkert Ventil

 

All three valve outlets are on the same level. Only the valve needs to be replaced during a service – no need to modify the piping.

 

 

Michael Landgraf, Geschäftsführer bei aprotec

“What’s more, the valves themselves are also vacuum-tight up to 1 × 10⁻⁷ mbar·l/s. With a nominal diameter of 4 mm, they allow for a high throughput despite their compact dimensions.”

Michael Landgraf, Managing Director at aprotec

Another practical feature proved to be beneficial: all three valve outlets are located at the bottom of the housing. This is an advantage over other valve variants where the third outlet is usually at the top. With all three outlets on the same level, the valve can be easily replaced during a service without needing to modify the piping. The developers of the tightness testing system and the manufacturer of the air conditioning units are both very satisfied, given that all measurement results are reproducible and well-documented, thanks in no small part to the valves. Campervan and motorhome owners can rely on their air conditioning systems functioning in summer and can rest assured that nothing will stand in the way of a stress-free summer holiday.

 

Michael Landgraf, Geschäftsführer bei aprotec

“For us, quality and reliability are paramount concerns for all components used, as we also maintain high quality standards for our systems.”

Michael Landgraf, Managing Director at aprotec
Form

Contact Sales

Christian Bürkert GmbH & Co. KG

Christian-Bürkert-Straße 13-17

D-74653 Ingelfingen, Germany

Telefon: +49 7940 10 0

Telefax: +49 7940 10-91 204

Do you have any questions? Don´t hesitate to contact us.