Share via email
Some fields are missing
send eMail
Speech bubbles
Customised Solution

Do you want to develop and realise a customised solution with us?

 Consulting

 E-Mail

 

Security for aggressive processes

Rugged conductivity sensors - the collaboration with RENA

Benefit from rugged conductivity sensors:

  • Safe processes: Thanks to the durable plastic valve body, the sensors are also suitable for use in aggressive ambient
conditions.
  • High flexibility: Various fittings, seals and nominal diameters allow for easy integration into different systems.
  • Monitor continuously: Conductivity sensors detect changes in concentration and report them to the controller, which automatically switches off the process and thus prevents consequential damage.
  • Simple start-up: The sensor fitting system ensures easy installation of the devices in all pipelines.

Durable conductivity sensors for wet chemical surface treatment

From wet chemical plants, where wafers for solar cells are manufactured or printed circuit boards are etched, to electroplating - such production processes require the use of aggressive acids and alkalis.

Therefore, the sensors must meet certain requirements, since common housing materials such as steel or stainless steel are not compatible with aggressive substances like these, which would cause the quick destruction of the materials To safely avoid contamination, ultrapure water requires inert sensors.

The solution lies in sensors for conductivity and flow measurement, with housings made from high-quality plastics such as PVDF or PP.

Rugged conductivity sensors for aggressive conditions

Thanks to the high-quality, chemically inert plastic materials deployed and specifically optimised for use in electroplating and wet chemistry, the sensors are ideally suited to be used under aggressive environmental conditions.

 

RENA Sensoren

Conductive conductivity measuring device for high-quality monitoring of ultrapure water. Source: RENA Technologies GmbH

Systems for wet chemical inline and batch processes

RENA, based in the German town of Gütenbach in the Black Forest, has long been a specialist in production facilities used in wet chemical surface treatment in solar, semiconductor and medical technologies. Its extensive and wide ranging product portfolio can be flexibly applied to a diverse range of manufacturing processes. Functionality, reliability and safety are at the heart of everything RENA does.

The wet-chemical inline and batch processes for solar cell production, for which RENA is the global market leader, are in use worldwide and have been working reliably and safely for many years. This places high demands on the components used. For example, on the sensors that are used for conductivity measurements when distributing demineralised water, or for monitoring heat exchangers during the etching process.

Reliable sensors in robust plastic valve bodies

Wet chemical process downtimes, e.g. for unplanned sensor replacements, must be avoided under all circumstances. That’s why the Black Forest-based manufacturers have placed their faith in our sensors in robust plastic valve bodies for many years.

RENA uses several inductive and conductive conductivity sensors in its wet chemical surface treatment plants.

 

Production systems for wet chemical surface treatment in solar technology. Source: RENA Technologies GmbH

Monitoring mixing ratios and cooling water circuits

Inductive conductivity measurement is the preferred method for determining the concentration of acids and alkalis. An alternating current flowing in the primary coil (transmitter) generates an alternating magnetic field. This induces a current in the surrounding ionically conductive medium. The current flow in the medium generates a magnetic field. This in turn generates a voltage and thus a current flow in the secondary coil (consumer) of the sensor. This is a measure of the medium’s conductivity.

Since the conductivity of fluids is significantly dependent on temperature, an additional temperature probe in the sensor continuously records the temperature of the medium. The temperature’s influence is compensated for via the temperature coefficient (TK value) set in the electronics assembly. Our Type 8228 inductive conductivity meter then provides this measured value to the controller as an interference-free 4... 20 mA signal, which can be easily transmitted over long distances in systems that are often very large.

These measuring devices perform two tasks in the wet-chemical surface treatment plants:

 

During etching processes, they monitor the cooling water circuit. In the (rare) event of a hole forming in the heat exchanger, for example, twenty percent hydrofluoric acid would penetrate the secondary circuit. Should such an event occur, the conductivity sensors detect the change in concentration and report it to the controller. Then controller then automatically switches off the process and thus prevents consequential damage. Another task for the inductive conductivity meters is to monitor the concentration of alkaline textures. Here, ensuring the correct mixing ratios is crucial for maintaining processing quality. The measuring devices operate within a large measuring range - from 100 μS/cm to 2 S/cm, with the resolution at 0.1 μS/cm.

The inductive conductivity meter in the circulation circuit of an etching process. Source: RENA Technologies GmbH

Conductivity measurement in demineralised water

Demineralised water, deionised water or ultrapure water is required for cleaning during wafer production. Its quality is also monitored in the wet chemical plants through conductivity measurement. Since this water’s conductivity is very low, this take is carried out by Type 8222 neutrino conductive measuring devices.

The device’s sensors consist of two electrodes in contact with the medium and a temperature probe, and they work is a measurement range of 0.05 μS/cm to 10 mS/cm. The measurement signal is also processed directly in the sensor. It is transmitted to the controller as an interference-immune 4...20 mA signal.

The conductivity meters have proven themselves in many applications, and RENA also relies on Bürkert solutions for other sensors that are required for wet chemical machining processes.

Precise inline flow measurement

The Type 8030 inline flowmeter or the Type 8035 inline batch controller are often used for continuous measurements of media supply or leakage monitoring. Both consist of a compact sensor fitting with an impeller and a transmitter. The connection is quick and easy thanks to a bayonet catch. Our sensor fitting system ensures simple and straightforward installation of the devices in all pipelines.

The sensors are suitable for use with flow velocities of 0.3m/s to 10m/s. The housings are made from PVDF or glass fibre-free PP and are completely leak-proof. They are also the perfect choice for use in the aggressive environment of wet chemical plants or electroplating processes.

Typ 8030 und Typ 8035

Inline flowmeters are used to continually measure media supply and to monitor for leakages, e.g. Type 8030 (left) or Type 8035 (right).

RENA Technologies GmbH - Sicherheit für aggressive Prozesse

Flyer Best Practice Durable conductivity sensors for wet chemical surface treatment

1.37 MB

 

Form

Contact Sales

Christian Bürkert GmbH & Co. KG

Christian-Bürkert-Straße 13-17

D-74653 Ingelfingen, Germany

Telefon: +49 7940 10 0

Telefax: +49 7940 10-91 204

Do you have any questions? Don´t hesitate to contact us.

 

My Comparison List