Share via email
Some fields are missing
send eMail
Speech bubbles
Customised Solution

Do you want to develop and realise a customised solution with us?

 Consulting

 E-Mail

 

Optimising the furnace atmosphere in heat treatment plants

Cooperation with Härterei Carl Gommann GmbH

How you benefit from Bürkert solutions for the heat treatment of steel

  • Better process reliability: successful cooperation for a plug-and-play solution ensuring a reproducible gas composition
  • Reliable operation: selected mass flow controllers ensure fast response times and a precise gas regulation
  • High level of flexibility: power supply and software function challenges solved quickly and efficiently

Increasing quality requirements, reproducibility, documentation and shorter delivery times coupled with a high degree of cost awareness – these are the challenges facing operators of heat treatment plants. Responsive mass flow controllers (MFCs) that are specially designed for precisely dosing large gas quantities offer advantages here. When experts in fluidics, control specialists and furnace designers work hand in hand, the user profits from the resultant plug-and-play complete solutions, which can easily connect to higher-level control equipment to provide exact dosing and logging of gas quantities. Thanks to excellent team work, Härterei Carl Gommann GmbH in Remscheid achieves greater process reliability for the heat treatment of steel.

Reproducible gas composition required

The material steel is renowned for its diverse technical applications. By adding alloy elements, it is possible to produce steels with different characteristics. In combination with different thermal treatments, the mechanical properties of the steel can be optimised to suit the respective machining and usage conditions. Härterei Carl Gommann GmbH specialises in the heat treatment processes of nitriding and nitrocarburizing as well as stress-relief annealing and the hardening and tempering of sheet metal. The company also develops sophisticated nitriding procedures for new materials and special alloys. Gommann purchases most of its heat treatment plants from the casting system and furnace builder KGO GmbH. STANGE Elektronik develops compact controls that are especially tailored to the needs of annealing furnaces. In the furnaces used for surface finishing, the products are hardened and tempered by exposure to heat and specific atmospheres. The gas compositions play a key role in the outcome of the heat treatment process — as do the temperatures. The gas quantities are fed in as specified by the control equipment via mass flow controllers because this is the only way to optimise the reproducibility of the gas composition and, therefore, the process reliability.

Precise regulation of gas supply

Furnace builders and control manufacturers place special requirements on mass flow meters: They need to operate very precisely, employ proven technology, be easy to network and robust – all without costing the earth. All these needs are met by Bürkert mass flow meters. The MFCs Types 8742/8746 can be calibrated for up to four gases. They are designed as compact devices incorporating the following components: flow rate sensor, control electronics as well as a proportional valve as an actuator. They guarantee very sensitive and precise control independent of disturbance variables such as pressure fluctuations or temporary flow resistances. The integrated PI controller and direct-acting proportional valve that serves as an actuator guarantee high response sensitivity. The sensor elements that come into direct contact with the media combine rapid response times and immunity to contamination. The new MFCs communicate directly with the STANGE control based on CANopen. This offered the prospect of cost savings and streamlining throughout the plant since there would be no need for an additional fieldbus.

Process reliability thanks to solution-based team work

However, it is often not just specifications and technical characteristics that determine the success of a project but also the capacity for team work, especially when so many companies are involved. Initial challenges relating to the power supply were also simply resolved thanks to the close cooperation between the project partners: the software specialists from the expert in fluidics were able to provide the still required operating mode “node guard” in next to no time. The high power consumption of the MFCs demands sufficient cable cross sections over long distances. Among other things, the use of a suitable intermediate feed for the power supply provided the solution. Ultimately, the MFCs delivered a plug-and-play complete solution for controlling the furnace atmosphere – a solution that could also be easily connected to the higher-level control equipment to ensure exact dosing and logging of the gas quantities.

Type 8742

Mass flow controller (MFC)/ mass flow meter (MFM) for gases

Type 8742
  • Nominal flow ranges from 0.010 l/min to 160 l/min
  • Highest measuring accuracy and repeatability with very fast response times
  • Long-term stability of the flow calibration
  • Easy device exchange due to configuration memory
  • Optional: ATEX II Cat. 3G/D or USP Class VI, FDA, EC 1935 conformity

Type 8746

Mass flow controller (MFC)/mass flow meter (MFM) for gases

Type 8746
  • Nominal flow ranges from 20 l/min up to 2500 l/min
  • High measuring accuracy and repeatability with very fast response times
  • Long-term stability of the flow calibration
  • Simpler device exchange due to configuration memory
  • Optional: ATEX II Cat. 3G/D or USP Class VI, FDA, EC 1935 conformity

Härterei Carl Gommann GmbH - Optimising the furnace atmosphere in heat treatment plants Best Practice

Flyer Best Practice Optimising the furnace atmosphere in heat treatment plants

194.17 KB

My Comparison List