Share via email
Some fields are missing
send eMail

Digital twins in the process industry: fluidics specialist Bürkert expands collaboration with Ascon Systems

Bereits seit 2021 arbeitet Bürkert Fluid Control Systems, ein weltweit führender Anbieter von Mess, Steuer- und Regelungstechnik für Flüssigkeiten und Gase, mit den Software-definierten Lösungen von Ascon Systems, einem Deep-Tech-Spezialisten für die Prozessautomation. Jetzt kommen bei Bürkert auch Digital Twins von Ascon Systems zum Einsatz. Sie erhöhen die Flexibilität und Effizienz bei verschiedenen Anwendungen der Kunden von Bürkert, weil sie unabhängig von Hardware Prozessdaten kontextualisiert speichern, bereitstellen und weiterverwenden und so die Steuerung der oft vielschichtigen Fluidiktechnik optimieren. Auf der Messe SPS in Nürnberg (12. bis 14. November 2024) demonstrieren Bürkert und Ascon Systems das Zusammenspiel der Technologien und zeigen das Potenzial.

Fluidics technology is precision work. It is used as a key technology in many sectors of industry whenever the flow of liquids or gases needs to be controlled. Applications can be found in the pharmaceutical, chemical, consumer goods and food industries and are increasingly common in areas of green engineering, such as fuel cell technology or bioreactors. The challenge in these systems is to deliver the exact amount of fluid in a precisely defined time and speed. Both the hardware, in the form of sensors, actuators and pumps, and the software must be able to meet these high standards of precision.

Bürkert is one of the world’s leading suppliers capable of providing such precision technology. In cooperation with Ascon Systems, Bürkert has so far transferred duties from hardware to software – in other words, IT goes OT. This has already enabled Bürkert to create a hardware-independent description of functions, model data flows and network data across systems and locations.

The two companies are now expanding their collaboration and taking the next step in software-defined production with the introduction of digital twins. The digital twins from Ascon Systems enable Bürkert to store, provide and reuse data in a contextualised manner. This means Bürkert can help its customers to configure and control applications. This enables them to leverage software to make hardware usable for multiple applications and to implement changing requirements, such as those arising from demand, product changes or new product launches, more quickly. This has a positive effect on time-to-market, while also increasing sustainability and improving the CO2 footprint Bürkert and Ascon Systems are now demonstrating what this high-tech interplay can look like at SPS in Nuremberg (details below).

Dr Anne März, Head of Digital Tool Chain at Bürkert Fluid Control Systems, says: “Digital twins are becoming increasingly popular for optimising production processes. Now, they are also becoming a reality in fluid technology. Ascon Systems technology helps to significantly simplify the creation and scaling of digital twins and their networking to the real world. This approach enables us to realise our customers’ requirements faster and more flexibly. Customers can think about and describe the desired application from their own perspective, while we translate it into a hardware-neutral solution using digital twin technology. Once a solution has been found, it is transferred to the real world and can be replicated for other locations and customised with other components on the hardware side. By expanding our collaboration with Ascon Systems, we are now in a position to rethink digital solutions. We also see great potential in this for the future.”

Jens Mueller, CEO from Ascon Systems, added: “Since we started establishing digital twins in industrial applications in 2017, the possibilities for deployment scenarios and applications in all industries have increased enormously. We are delighted that we can now extend our long-standing, trusting cooperation with Bürkert to the area of digital twins. Together, we can show how software-defined precision technology can lead to greater efficiency, sustainability and cost reductions in hardware too. We believe this transformation is one of the most important opportunities for companies to position themselves resiliently for the future in global competition.”

Ascon Systems and Bürkert at SPS in Nuremberg

The SPS (Smart Production Solutions) trade fair will take place in Nuremberg from 12 to 14 November 2024. Ascon Systems and Bürkert will each be represented with a stand. You are cordially invited to come by for a demonstration of the joint technology.

To make an appointment, please contact
Jürgen van Santen, +49 7940 10 91 302, juergen.vansanten@burkert.com
Michael Polaczy, +49 151 729 675 28, michael.polaczy@ascon-systems.de  


Ascon Systems, Hall 6, Stand 117:
Presentation “The factory of the future is more than virtualisation”: Jens Mueller, CEO Ascon Systems, Tuesday, 12 November 2024, 11:20 to 11:40 a.m., Hall 6, Forum

Bürkert Fluid Control Systems, Hall 7, Stand 360:
Example concept “Virtual calibration: how digital twins can fundamentally change processes in the future.”

https://www.buerkert.de/de/unternehmen-karriere/aktuelles/news/buerkert-sps-2024
https://www.burkert.com/en/landingpage/digital-twin-for-automation-and-amp-digitalisation-strategy

Press release for editors: