Share via email
Some fields are missing
send eMail

Revolutionary flow measurement concept for the Pharmaceutical industry

John van Loon, Application Manager Hygienic
Marc Klingler, Application Manager Hygienic

Fluid flow measurement technology is designed to improve productivity and provide crucial information for manufacturing processes. Within the Pharmaceutical industry it is also required to perform to exacting stand-ards relating to hygiene, purity and accuracy that will meet both internal targets and the regulatory requirements. Liquid flowmeters are used throughout pharmaceutical processes, with the majority of the high specification meters being used in the production of the Active Pharma-ceutical Ingredient (API). All of these flowmeters have limitations leading to designers having to make a compromise in many cases.