Zero switch-off function

The zero switch-off function ensures that the valve is closed if the input signal is less than 2 % of the maximum value.

Print

The coil current is then set to zero. The zero switch-off function must generally be deactivated to set the minimum coil current.

My Comparison List