Chemical seal

Used for pressure measurements.

Graphic illustration of a chemical seal

A chemical seal consists of a chamber filled with a transfer fluid (oil-based mixture), closed on one side by a pressure sensor and closed off from the process on the other by means of a diaphragm (stainless steel or plastic). The pressure bends the diaphragm and is transferred from the fluid to the pressure sensor.

Chemical seals are used if the process conditions no longer allow direct attachment of a pressure sensor (extreme temperatures, chemical resistance, hygienic requirements or media which form coatings or are very viscous etc.).

A wide range of process connections also allows use in special applications.

My Comparison List