Share via email
Some fields are missing
send eMail
bürkert
 

Automation, central

Automation concept

In the case of central automation, the pneumatic auxiliary energy is switched in the control cubicle, normally by a valve block with field bus interface or by the AirLine pneumatic automation system, and routed to the valve actuator with pneumatic control lines. The electrical feedback signals from the process valve are also routed to the control cubicle.

Control Cabinet SolutionsControl Cabinet Solutions

Control cabinets can contain many diverse components, depending on the application. Starting with 2 valves mounted in a small plastic control box, to control cabinets with combined pneumatic, electronic and valve technology, all the way to highly complex customized system panels with control functions in a stainless steel housing, Bürkert – as a competent system supplier – offers a broad spectrum of control cabinet solutions.

Form

Contact Sales

Christian Bürkert GmbH & Co. KG

Christian-Bürkert-Straße 13-17

D-74653 Ingelfingen, Germany

Telefon: +49 7940 10 0

Telefax: +49 7940 10-91 204

Do you have any questions? Don´t hesitate to contact us.

My Comparison List