Turbidity measurement now also according to US EPA

Bürkert's online analysis system Type 8905 is a modular system for monitoring all important water parameters on one platform. In the basic version, five measurement parameters are provided as independent sensor cubes: pH value, redox potential (ORP), conductivity, free chlorine and turbidity. Turbidity measurement is now also offered according to US EPA.

The MS05 sensor cube for turbidity measurement was designed by Bürkert for operation on the fluidics backplane in the Type 8905 Online Analysis System. The continuous analysis of turbidity in water is the indicator for undesirable undissolved substances in water. The measurement can, for example, display the filter effect and thus enables the optimization of the filter stage including integrity tests. This can even lead to water and energy savings.

My Comparison List