Strategic alliance for automating your process

Bürkert and Siemens combine their expertise

Valve island Burkert

Maximum system availability and process reliability for pneumatic controllers is the goal of a strategic partnership between Bürkert and Siemens. The result of the cooperation is the new Type 8647 AirLINE SP valve island, which is compatible with the Siemens I/O system SIMATIC ET 200SP. Bürkert will present the valve island system at SPS IPC Drives in Nuremberg from 22 to 24 November 2016.

The highly versatile valve island was developed for use in the food & beverage, pharmaceuticals and cosmetics industries, as well as in water treatment systems. To save space it can be mounted in the control cabinet together with different Siemens modules for controlling up to 64 valve functions. The valves are directly connected to the Siemens I/O system. This enables fast and seamless integration both at the time of commissioning and later, during monitoring of operation. The display of the number of switching cycles allows optimal preventive maintenance of the system to minimise wear and downtimes. Maximum system availability is achieved by means of the pneumatic valves in the supply channel: they are hot swap capable, so they can be replaced during operation.

Press Release:

My Comparison List