Precise monitoring of drinking water disinfection with Online Analyse System

The Bürkert Online Analysis System can now measure chlorine dioxide

Bürkert has expanded the Type MS02 sensor cube for the Type 8905 Online Analysis System. The system can now measure either free active chlorine or chlorine dioxide. The Online Analysis System is designed for automatic monitoring of the most important analysis parameters in the treatment of drinking water.

The Type 8905 Online Analysis System from Bürkert is a modular system for fully automatic monitoring of all important water parameters with a single platform. The basic version provides sensor cubes for five parameters: pH value, redox potential (ORP), conductivity, chlorine and turbidity. Measurement of the chlorine dioxide content expands the capabilities of the Online Analysis System to include yet another important parameter. Precise amounts of chlorine dioxide are added to drinking and process water for disinfection purposes. The chlorine dioxide sensor makes it possible to continuously monitor and document the concentration and the effectiveness of the disinfection.

Press release:

My Comparison List