More flexibility: Bürkert's multiCELL transmitter / controller type 8619 will be available in a new housing version and optional 110/230 VAC supply starting in June 2014
Bürkert's modular multi-channel multiCELL transmitter/controller type 8619 is a customisable measuring system with an extended range of functionalities that can work with multiple types of sensors. With this new variant, fluid technology specialist Bürkert will extend the scope of their type 8619 which has been available only for panel installation so far. Starting in June, there will be a new, separate housing version which will offer more flexibility in installation, for example on walls, railings or pipelines. The new variant can be supplied with a 12…36 VDC supply, as before, or alternatively with 110 / 230 VAC supply.

With multiCELL transmitter/controller type 8619, Bürkert offers a complete and flexible measuring system suitable for connecting multiple sensors for the most diverse range of tasks in data logging, control and dosing. The device is perfect for numerous applications in areas as diverse as water treatment or the production of foodstuffs and pharmaceutics. The system consists of a basic device which comes with generous equipment, but whose functional range can be freely adapted and extended, as required, with hardware boards for pH / ORP, conductivity, input + output signal boards and software modules. Bürkert's multiCELL type 8619 is now available not only in a version for panel installation, but also with a housing, offering users more flexibility in the installation of the device, e.g. on walls, pipelines and railings.
Peter Feneberg