First standard cartridge valve from Bürkert

The new cartridge valve (Type 6164) from Bürkert simplifies pneumatic piloting controls through optimal integration of a pilot valve in block solutions and plastic injection moulded components.

Print

Install and forget – this is the best way to describe the new standard cartridge valve from Bürkert. The fluidics engineers from Ingelfingen have developed a 3/2-way valve with guaranteed reliability and a long life cycle, due to the use of high-quality materials. The compact size of the cartridge valves makes them ideal for the use within block solutions, in which case the valves do not have to be mounted completely on the blocks; instead, they can easily be integrated via “plug and play”.

First standard cartridge valve from Bürkert

Due to the increasing importance of space considerations, fluid performance and energy saving potentials, customised solutions are constantly becoming more complex, accompanied by higher component requirements. The new cartridge valve (Type 6164) from Bürkert simplifies pneumatic piloting controls through optimal integration of a pilot valve in block solutions and plastic injection moulded components. Due to its uncompromising reliability, above-average service life and efficient performance, this valve is setting new standards.

Press release

My Comparison List