Share via email
Some fields are missing
send eMail
bürkert
 

Bürkert @ COMPAMED 2022

Visit us from November 14 to 17, 2022 in Hall 8b, at booth H07 and find more information about customized fluid management systems for your medical technology application.

Customized system solutions for your application –
Focus on your core business, we take care of the fluidics!

By outsourcing a sub-process to a trustworthy and reliable partner, you create space for yourself in which you can fully focus on your core business - e.g. the optimization of your medical devices.

We provide you with the fluidic system solution, from the idea to development and production. Due to our high vertical range of manufacture, we are usually able to deliver even in these difficult times.

Bring your challenge to COMPAMED. We look forward to a personal discussion with you!

You don't have an vochure code for COMPAMED yet?

Then please contact us at: Contact Event

You already have a personal voucher code?
You can enter it here: www.compamed.com/vochure

Please observe the Covid rules in force at the time of the fair.

This is what you can expect at COMPAMED:

  • System solution for dosing small quantities
  • System solutions for in vitro diagnostics
  • System solution from the field of stem cell research
  • System solution for respiratory technology
  • System solutions for personalized medicine
  • Energy-saving pulse valve Type 6724
  • Durable and reliable components such as microvalves, pressure controller

 

In Vitro Diagnostic (IVD) solutions: Precision, automation and increased throughputIn Vitro Diagnostic (IVD) solutions: Precision, automation and increased throughput

The precision and accuracy of the analyses determine the diagnosis. These requirements apply in particular to critical applications such as haematology, clinical chemistry, flow cytometry, immunology or histology. At the same time, the speed and the space required for the device in the laboratory are essential for in-vitro diagnostics due to the rapidly increasing need for tests. Bürkert has the right solution for both.

Scientific research handling and dosing in the micro rangeScientific research handling and dosing in the micro range

We blend your specialist knowledge with our comprehensive know-how. This results in solutions that are perfect down to the very last detail and help to reduce complexity. Since we give your idea the respect and attention it deserves – irrespective of whether you work with stem cells or dose micro-litres. Be inspired by the following real success stories and discover how we build on and increase the knowledge of our clients. Ensuring everything flows smoothly all of the time.

Creative Eurecom - system partnership for the development of a medical device for home use

Flyer Best Practice - ALX-009: Systems partnership for the development of a medical device for home use - treatment of cystic fibrosis.

2.42 MB

How innovative dosing systems make liquid chromatography more accurateHow innovative dosing systems make liquid chromatography more accurate

As a user of a chromatography device, you know: Only if substances from the pharmaceutical or clinical environment or from the environment and forensics can be analysed exactly and quickly in the chromatograph can you work really efficiently and ensure fast further processing. The precision in the dosage also determines how well you can automate your processes.

Type 6724

2/2 or 3/2-way Whisper Valve with media separation

Type 6724
  • Highest chemical resistance
  • Compact design with 8.9 mm installation width
  • DN 0.8 mm (vacuum up to 5 bar) and 1.2 mm (vacuum up to 3 bar)
  • Very fast, almost silent switching with < 20 dB (A) and very low power consumption
  • High back-pressure tightness, excellent cleanability and 100% duty cycle

Type 8763

Pressure controller for precise time-pressure dosing

Type 8763
  • Repeatable and accurate dosing of liquids in the µl range
  • Response time in milliseconds and active pressure relief for optimum control performance
  • Digital communication for easy integration into your fieldbus network
  • Extended functionality through additional sensor input + actuator output e.g. for pump or additional pressure sensor
  • Active vent valve to minimize consumption of costly carrier gas

 

Our system solutions are developed in the five Buerkert-Systemhauses in Germany, the USA and China. Experienced project teams work closely with you to develop individual solutions tailored to your needs.

My Comparison List